The Symbol Quality menu shows commands that allow you to define the evaluation of symbols per the ISO/IEC 16022 specification, or by a collection of commonly-used grading parameters. The two Global commands allow you to define the separator that will appear between instances of symbol quality output, and the format in which symbol quality evaluations will be output.
Command parameters can be changed directly from this menu.

Important: For descriptions of symbol grading functionality, refer to the Symbol Grading section in I/O.