Start

The Start view is the initial view you will see when the WebLink session begins. The connected reader is shown, along with its user-defined name, IP address, Reader Model, Serial Number, MAC ID, Firmware version, WebLink version, Sensor, and Optics.

 

Note: The user-defined name must be 19 characters or fewer.

 

This view allows you to choose Assisted Setup, to Create a New Setup, or to Load a Setup.

 

 

Click the gear icon at the upper right to bring up the Application Settings menu. This menu includes several functions: Save, New, Load, Advanced, Language, Terminal, Beeper, Guided Tour, Image Storage, Restore Default Settings, Active Account Management, and About WebLink.

 

Note: The Enable USB Drive Mode options only appears when you are using a device that supports USB connectivity.

 

 

Clicking About WebLink opens the dialog shown below, which shows the current WebLink version, Reader Model, Serial Number, Part Number, MAC ID, Sensor, Firmware version, Boot version, Browser, Operating System, and Screen Resolution.

 

Note: The information in this dialog is selectable so that you can copy it to a clipboard.

 

Clicking Contact us... takes you to the Omron Microscan website.