The Setup view allows you to configure all aspects of a setup. Multiple discrete sections of the interface give you the ability to set Autocalibration, Cycle, Acquire, Decode, Match String, Format Output, Output parameters, and Favorites.
Clicking the flash icon at the upper right saves current settings to the reader’s flash memory so the settings will be available when the reader is rebooted.
The question mark icon at the upper right opens WebLink Help.

The gear icon at the upper right brings up the Application Settings menu. This menu includes several functions: Save, New, Load, Advanced, Language, Terminal, Beeper, Guided Tour, Image Storage, Restore Default Settings, Manage Login, Enable USB Drive Mode, and About WebLink.
Note: The Enable USB Drive Mode option only appears when you are using a device that supports USB connectivity.

Click About WebLink to display your current WebLink version, Reader Model, Serial Number, Part Number, MAC ID, Sensor, Firmware version, Boot version, Browser, Operating System, and Screen Resolution.
Clicking Contact us... takes you to the Omron Microscan website.