Bring up the Output 1, Output 2, and Output 3 dialogs by clicking on the Outputs section at the lower left of the Setup view. For each output you can determine the Output On behavior, Mode, Pulse Width, and State. Outputs 2 and 3 also allow you to determine output behavior based on Trend Options parameters or Symbol Quality Options parameters.
This example shows the dialog that appears when you click Symbol Quality Options. A similar dialog would also appear for Trend Options under Output 2.
Note: The 1, 2, and 3 output indicators at the lower right of the screen display the results of the last read cycle.

Output On provides discrete signalling to host software to control external devices such as PLCs and relays. It is useful for routing, sorting, and to prevent mis-packaging and mis-routing. This option allows you to set the conditions under which an output (or outputs) will be activated.

Output Mode sets the condition in which the discrete output is de-activated.

Pulse Width sets the time in milliseconds that the discrete output remains active.

Output State allows you to set the active electrical state of the discrete output to Normally Open or Normally Closed.

Triggered Outputs show when outputs are triggered and give you the ability to trigger outputs manually.
Outputs 1 - 3 are located in the lower right corner of the user interface. They function both as buttons that trigger whichever output you click, and as a display that shows which output is currently being triggered. In the example below, output 2 is being triggered.
Note: The three output indicators shown below display the results of the last read cycle.