Note: Match String can only be used in Triggered, Start/Stop, and Custom modes. It cannot be used in Presentation or Continuous modes.
The Match String menu shows all the commands that allow you to determine the type of matching behavior required of the reader, as well as new master pin functionality (enabled or disabled), and the character strings intended to replace a string of decoded data that is either a match or mismatch with the user-defined match string.
Command parameters can be changed directly from this menu.