Left Panel

The area to the left of the Image Area is different depending on whether you are in the Start or Setup view. (In the Run view, the Image Area expands and the left panel is not present.)

 

Left Panel in Start View

In the Start view, the left panel shows your reader's user-defined name, IP address, Reader Model, Serial Number, MAC ID, Firmware version, WebLink version, Sensor, and Optics.

 

Note: The user-defined name must be 19 characters or fewer.

 

The left panel in the Start view also contains buttons for Assisted Setup, Create a New Setup, and Load a Setup.

 

 

Left Panel in Setup View

In the Setup view, the left panel contains the majority of WebLink's configuration tools: Cycle, which allows you to set the trigger mode; Acquire, which allows you to set the camera's exposure and gain; Decode, which allows you to select which code types are required in your application; Match String, which allows you to set the match code mode, wildcard, text output, new master, and match string database; Format Output, which allows you to determine the ways in which barcode data can be formatted before it is output as a data string; Outputs, which allows you to determine output conditions, the output mode, the pulse width, and the output state (normally open or normally closed); and Favorites, which allows you to define the commands you use most frequently and gives you quick access to their command parameters.