When you click the Image Storage icon in the Application Settings menu, you will see this dialog:

When you turn Image Storage on and click OK, the dialog will expand as shown below. The Image Storage Options dialog shows commands that allow you to control how, when, and where images captured by the camera are stored.

If Image Storage Location is set to Remote (FTP), the FTP Address will appear, allowing you to input the user ID, password, and address of the applicable FTP server.

If the RAM drive size changes, the message shown below will appear in the Image Storage Location dialog.
If you click Revert, the RAM drive size returns to its previous size.

All Image Storage settings can also be configured in Advanced Settings.
An external FTP server can be used to store images captured by the reader. The reader can connect to an FTP server and can send images and cycle reports to that server for storage. The following procedure describes how to set up an external FTP server.
The example procedure shown here uses FileZilla Server, which can be downloaded at https://filezilla-project.org/. Note that FileZilla is a Windows-only utility.

Connect to the server. Use the 127.0.0.1 server address if you are setting up the server on your PC. Note the port that you use – 14147 in the example shown here – as the port number will be required when you log back into the server.






Note: pwd represents the password you set on the General page of the FileZilla Server interface.

During FileZilla installation, you have the option of configuring FileZilla Server to auto-start each time the reader is powered on. You can also start and stop the server manually via the Start FileZilla Server and Stop FileZilla Server shortcuts shown here.

To disable FileZilla Server's auto-start feature: