Note: The Enable USB Drive Mode option only appears in the Application Settings menu when you are using a V420-F, which supports USB connectivity.
Clicking Enable USB Drive Mode in the Application Settings menu brings up the Enable USB Drive Mode dialog shown below.

When you click the Enable button in the dialog, your reader will reboot, and then you can use it as you would a USB flash drive. If you click Enable - Don't Reboot, the camera will reboot later.
Important: The USB drive functionality self-disables on the next reader reboot. To enable USB drive functionality again, follow the same procedure described above.

If you try to enable USB Drive Mode when it's already enabled, this dialog will appear: