Camera Setup

The Camera Setup menu shows all the commands that control the function of the reader's camera. Many of these command settings can also be controlled from the WebLink user interface. For example, the Exposure and Gain settings in the Camera Settings command can be configured in the Acquire section located in the left panel of the Setup view.

 

Command parameters can be changed directly from this menu.

 

Camera Setup Menu

 

Note: When Illumination Brightness is set to Constant, the illumination brightness is the same power level as the High setting. However, the LEDs are continuously on once Brightness is set to Constant, and they will remain on during and after the read cycle to eliminate perceptible flashing.

 

 

Power Strobe Mode and External Strobe

 

 

Power Strobe Mode

 

Activate Power Strobe mode by setting Illumination Brightness to Extreme and setting Light Source to External Strobe.

 

 

External Strobe

 

External Strobe is part of the Light Source parameter.

 

 

Fixed Light On Time and Fixed Light Delay Time

 

Fixed Light On Time and Fixed Light Delay Time are only valid when Illumination Brightness is set to Extreme.

 

 

Use as External Illumination Strobe

Use as External Illumination Strobe is available in the Output On parameter of the Output 3 command in I/O Parameters. External Strobe must be enabled for this parameter to function.

 

 

 

Lighting Mode Table