Click the gear icon to the right of the help icon to open the Application Settings menu. One of the options you will see is Advanced.


WebLink's Advanced settings allow you to make fine adjustments to individual command parameters in all areas of your reader's functionality: Camera Setup, Communications, Read Cycle, Symbologies, I/O, Symbol Quality, Match String, Diagnostics, Image Storage, and Configuration Database. Many of these commands can be configured directly in the WebLink user interface, but all parameters can be configured and examined in Advanced settings.
Advanced settings are an efficient way to send complex, multi-parameter commands to the reader.
Each menu of Advanced settings commands is shown in the following sections, and an additional section is included that shows an example of the Differences from Default menu, which shows only commands that are different from WebLink defaults.